Enerlin'X Devices Compatible with MTZ MicroLogic X Control Unit
NOTICE |
---|
HAZARD OF NON-COMMUNICATION BETWEEN the IMU DEVICES
Check the firmware compatibility of the devices in the
IMU by using the latest version of
EcoStruxure Power
Commission
software, and follow the recommended actions.
Failure to follow these instructions can result in critical
firmware discrepancy.
|
The following table shows the minimum firmware version of Enerlin'X devices that is required to enable communication with an MTZ MicroLogic X control unit.
Device | Part number | Firmware version of MTZ MicroLogic X control unit | |
---|---|---|---|
001.000.200 to 001.000.206 | ≥ 002.000.002 | ||
IFM Modbus-SL interface for one circuit breaker with RJ45 |
LV434000 |
≥ 003.000.012 |
released version > 003.001.000 |
IFM Modbus-SL interface for one circuit breaker |
TRV00210 STRV00210 |
– |
– |
IFE Ethernet interface for one circuit breaker with RTC |
LV434001 |
– |
≥ 003.007.024 |
IFE Ethernet interface for one circuit breaker |
LV434010 |
≥ 003.005.003 and date code ≥ HL16485 (1) |
≥ 003.007.024 |
IFE Ethernet switchboard server with RTC |
LV434002 |
– |
≥ 003.007.024 |
IFE Ethernet switchboard server |
LV434011 |
≥ 003.005.003 and date code ≥ HL16485 (1) |
≥ 003.007.024 |
EIFE Embedded Ethernet interface for one MasterPacT MTZ drawout circuit breaker |
LV851001 |
≥ 003.005.003 |
≥ 003.007.024 |
IO input/output application module for one circuit breaker |
LV434063 |
≥ 003.002.002 and date code ≥ HL16486 (2) |
≥ 003.003.011 |
FDM121 front display module for one circuit breaker |
TRV00121 STRV00121 |
≥ 004.000.009 |
≥ 004.000.009 |
FDM128 Ethernet display for eight devices |
LV434128 |
≥ 6.3.4 |
≥ 6.5.3 |
(1) IFE hardware is compatible if manufacturing date code on the IFE label is greater than HL16485. IFE hardware with manufacturing date code lower than HL16485 operates correctly but generates a non-critical hardware discrepancy. (2) IO module hardware is compatible if manufacturing date code on the IO module label is greater than HL16486. IO module hardware with manufacturing date code lower than HL16486 operates correctly but generates a non-critical hardware discrepancy. |
Example: An MTZ MicroLogic X control unit with firmware version 001.000.200 is compatible with:
-
IFM interface LV434000 with firmware version greater than or equal to 003.000.012
-
IFE interface with firmware version greater than or equal to 003.005.003 and date code greater than or equal to HL16485
-
EIFE interface with firmware version greater than or equal to 003.005.003
-
IO module for one circuit breaker with firmware version 003.002.002 and date code greater than or equal to HL16486
-
FDM128 display with firmware version greater than or equal to 6.3.4
The MTZ MicroLogic X control unit must be updated to firmware version greater than or equal to 002.000.002 to be compatible with an IFE interface with RTC.
NOTE: To benefit from the latest IMU features, it is recommended to update the firmware of the MTZ MicroLogic X control unit and the Enerlin'X devices of the IMU.