DOCA0155EN-11

Digital Modules Compatible with MTZ MicroLogic X Control Unit

The following table presents the minimum MicroLogic X firmware version needed for the Digital Module to function:

Digital Module Part number Firmware version of MTZ MicroLogic X control unit

IEC 61850 for MasterPact MTZ

LV850046

≥ 004.101.000

Directional overcurrent protection

LV850015

≥ 004.101.000

IDMTL overcurrent protection

LV850037

≥ 004.101.000

Under/Overfrequency protection

LV850013

≥ 003.012.000

Individual harmonics analysis

LV850006

≥ 002.000.002

Under/Over voltage protection

LV850012

≥ 002.000.002

Reverse active power

LV850011

≥ 002.000.002

Ground-fault alarm

LV850007

≥ 002.000.002

Energy Reduction Maintenance Settings (ERMS)

LV850009

≥ 002.000.002

Modbus legacy dataset

LV850045

≥ 002.000.002

Energy per phase

LV850002

≥ 001.000.002

Power restoration assistant

LV850004

≥ 001.000.002

MasterPact operation assistant

LV850005

≥ 001.000.002

Waveform capture on trip event

LV850003

≥ 001.000.002

Refer to DOCA0102EN MasterPact MTZ – MicroLogic X Control Unit – User Guide for compatibility of the Digital Module with Enerlin'X devices.

QR code for this page

Was this helpful?