DOCA0155EN-13

Procedure for Finding the Firmware Version of a MicroLogic Trip Unit or Control Unit

Follow this procedure to find the firmware version of a MicroLogic trip unit or control unit. The example shows the MicroLogic X control unit:

Step Action

1

Connect the PC running EcoStruxure Power Commission software to the MicroLogic trip unit or control unit.

2

Click Connect to device directly.

3

Fill in the project details and click NEXT.

4

Fill in the end user site details and click CONTINUE.

The device is displayed.

5

If a new MicroLogic X firmware version is available, a blue pop-up message is displayed to invite the user to update the firmware. Click CONNECT TO DEVICE.

6

Click Firmware.

The firmware versions of the devices in the IMU are displayed.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?