Airflow Values
Indicative Airflow Values in m3/Hour Based on a 30 °C Environment
Indicative Airflow Values in m3/Hour Based on a 40 °C Environment
UPS rating | 200 kW | 250 kW | 300 kW | 350 kW | 400 kW | 450 kW | 500 kW |
---|---|---|---|---|---|---|---|
50% load |
1920 |
2299 |
2678 |
3056 |
3435 |
3814 |
4193 |
75% load |
2284 |
2753 |
3223 |
3693 |
4163 |
4774 |
5284 |
90% load |
2465 |
2981 |
3496 |
4112 |
4668 |
5224 |
5860 |
100% load |
2647 |
3208 |
3769 |
4471 |
5072 |
5754 |
6416 |