990-91377B-001

EPO

EPO Configurations (Terminal J6600, 1-9)

The EPO input supports 24 VDC.

NOTE: The default setting for the EPO activation is to turn off the inverter.

If you want the EPO activation to transfer the UPS into forced static bypass operation instead, please contact Schneider Electric.

QR code for this page

Was this helpful?