990-91377B-001

Classic Battery Cabinet Runtimes for 400 V

Battery runtimes are listed in minutes at 100% load. Battery runtimes are estimated values based on battery manufacturer data for operation at 25 °C.

Please note that not all battery solutions are available for all UPS ratings due to:

  • The number of battery blocks in the specific battery solution differs from the specific UPS requirements.

  • The specific battery solution would provide less than 5 minutes runtime with the specific UPS.

  • The battery breaker rating in the specific battery solution does not match the specific UPS rating.

UPS rating 200 kW 250 kW 300 kW 350 kW 400 kW 450 kW 500 kW
Power factor 1
2 x GVSCBC10A2 7.9 5.4
2 x GVSCBC10B2 12.5 8.5 6
3 x GVSCBC10A2 14.0 10.0 7.9 6.1
3 x GVSCBC10B2 22.5 16.5 12.5 9.7 7.6 5.9
4 x GVSCBC10A2 21.0 15.0 12.0 9.7 8.0 6.5 5.4
4 x GVSCBC10B2 33.5 25.0 19.5 15.5 12.5 10.0 8.6
QR code for this page

Was this helpful?