990-5913D-001

Connect the Signal Cables to the Galaxy VL UPS

NOTE: Route the signal cables separately from the power cables to ensure sufficient isolation.
NOTE: Use double isolated signal cables. The signal cables must have a minimum rating of 600 V.
  1. Install the temperature sensor(s) 0M-1160 provided with the UPS in the top of the classic battery cabinet(s).
    WARNING
    Hazard of fire
    Position the temperature sensor as described to ensure correct temperature measurements.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    GVSCBC10A2, GVSCBC10B2

  2. Route the battery temperature sensor cables through the bottom of the classic battery cabinet to the UPS and connect as shown.
    NOTE: Two temperature sensors are provided with the UPS.
    NOTE: The battery temperature sensor cables are considered Class 2 and SELV. Class 2 and SELV circuits must be double isolated from the primary circuitry.
  3. Remove the cover on the battery breaker.
  4. Connect the signal cables to the battery breaker:
    1. Connect the signal cables to the AUX switch.
    2. Connect the signal cables to the undervoltage trip coil.
    3. Route the signal cables out through the lower opening of the battery breaker.
  5. Route the signal cables from behind the battery breaker and out through the bottom of the classic battery cabinet.

    Rear View of the Battery Breaker

  6. Reinstall the cover on the battery breaker.
  7. Connect the signal cables in the UPS as shown.
QR code for this page

Was this helpful?