990-91376E-001

Final Installation

  1. Only for dual mains: Add the labels for SSIB, the indicator lights, and the diagram label on the maintenance bypass cabinet. The labels are provided with this manual.

    Single Mains

    Dual Mains

  2. Add label 885-91965 (provided with the UPS) on the maintenance bypass cabinet.
  3. Only for seismic anchoring: Install the seismic front anchoring bracket on the maintenance bypass cabinet and on the UPS. Mount the seismic front brackets to the floor. Use appropriate hardware for the floor type – the hole diameter in the seismic front bracket is ø14 mm. The minimum requirement is M12 strength grade 8.8 hardware.
  4. Close the front door on the maintenance bypass cabinet
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?