990-91379B-001

Configure the Display Preferences

  1. Tap Configuration > General > Display.
    1. Set the temperature unit to Celsius or Fahrenheit.
    2. Tap the - or + to set the display brightness.
    3. Set the Alarm sound to Enable or Disable. This will enable/mute all alarm sounds.
    4. Set the Touch screen sound to Enable or Disable. This will enable/mute all display sounds (excluding alarm sounds).
QR code for this page

Was this helpful?