990-91399A-001

Airflow Values

Indicative Airflow Values in m3/Hour Based on a 30 °C (86 °F) Environment

UPS rating 200 kW 250 kW 300 kW 350 kW 400 kW 450 kW 500 kW
50% load

1617

1920

2223

2526

2829

3132

3435

75% load

2102

2526

2950

3375

3799

4223

4749

90% load

2344

2829

3314

3799

4365

4911

5436

100% load

2405

2905

3405

3905

4547

5087

5709

Indicative Airflow Values in m3/Hour Based on a 40 °C (104 °F) Environment

UPS rating 200 kW 250 kW 300 kW 350 kW 400 kW 450 kW 500 kW
50% load

1920

2299

2678

3056

3435

3814

4193

75% load

2284

2753

3223

3693

4163

4774

5284

90% load

2465

2981

3496

4112

4668

5224

5860

100% load

2647

3208

3769

4471

5072

5754

6416

QR code for this page

Was this helpful?