990-91399A-001

Hardware Options

NOTE: All hardware options listed here may not be available in all regions.

Power Module

  • Power module 50 kW (GVPM50KD)

Lithium-ion Battery Cabinet

Battery cabinet including Lithium-ion batteries and battery breaker.

  • Galaxy Lithium-ion battery cabinet with 16 battery modules (LIBSESMG16UL)

  • Galaxy Lithium-ion battery cabinet with 17 battery modules (LIBSESMG17UL)

  • Galaxy Lithium-ion battery cabinet with 17 battery modules (LIBSESMG95GUL)

  • Lithium-ion battery rack with 16 modules Type E (LIBSESMG95EUL)

  • Galaxy Lithium-ion battery cabinet with 17 battery modules (LIBSESMG95GUL1PH)

  • Galaxy Lithium-ion battery cabinet with 16 battery modules (LIBSESMG95EUL1PH)

  • Galaxy Lithium-ion battery cabinet with 17 battery modules (LIBATTSMGGUL)

  • Lithium-ion battery rack Type E (LIBATTSMGEUL)

Maintenance Bypass Cabinet

Maintenance bypass cabinet for complete isolation of the UPS during service operations. Only for single UPS.

  • 200-500 kW maintenance bypass cabinet with backfeed (GVLMBCA200K500G)

Bottom Entry Cabinet

Bottom entry cabinet for cable entry through the bottom of the system.

  • Bottom entry cabinet (GVBEC)

Optional Installation Kits

  • Seismic kit for UPS (GVLOPT002)

  • Backfeed kit for UPS (GVLOPT003)

  • Parallel kit for UPS (GVLOPT006)

  • SKRU kit (GVSOPT004)

Optional Network Management Card

  • Network Management Card LCES2 with Modbus, Ethernet and AUX sensors (AP9644)

Air Filter

  • Performance air filter kit for UPS (GVLOPT001)

Temperature Sensors

  • Temperature sensor for network management card (AP9335T)

  • Temperature/humidity sensor for network management card (AP9335TH)

QR code for this page

Was this helpful?