990-91734A-001

Connect the Power Cables in a Single Mains System

NOTE: The DC cables were connected during Position and Interconnect the Transformer Cabinets and the UPS.
  1. Route the EGC cable through the top or the bottom of the transformer cabinets and connect to the ground busbar.
  2. Route the input cables through the top or the bottom of the input transformer cabinet and connect to the input busbars (L1, L2, L3).
  3. Connect the provided UPS input cables 0W20107 from the UIB breaker to the terminals (L1, L2, L3) in the right side of the input transformer cabinet.
  4. Route the output cables through the top or the bottom of the output transformer cabinet and connect to the output busbars (L1, L2, L3, N).

    Top Cable Entry

    Bottom Cable Entry

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?