990-91734A-001

Decommission or Move the Transformer Cabinets to a New Location

NOTE: Follow the instructions in the UPS installation manual to prepare the UPS for being moved/decommissioned.
  1. Shut down the UPS system completely.
  2. Lockout/Tagout all breakers in the input transformer cabinet(s) in the OFF (open) position.
  3. Lockout/Tagout all breakers in the output transformer cabinet in the OFF (open) position.
  4. Lockout/Tagout all breakers in the upstream switchgear in the OFF (open) position.
  5. Lockout/Tagout all battery breakers in the switchgear/battery solution in the OFF (open) position.
  6. Open the front doors of the transformer cabinets and the UPS.
  7. If present, Lockout/Tagout the backfeed breaker BF2 in the OFF (open) position on the UPS.
  8. Remove the two plates from each of the transformer cabinets.

    Single Mains UPS System

    Dual Mains UPS System

  9. On the transformer cabinets, measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent plate for input, bypass, output, neutral. Reinstall the plates covering the measurement points on the transformer cabinets.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent plate for input, bypass, output.
    Failure to follow these instructions will result in death or serious injury.

    Single Mains System

    Dual Mains System

  10. On the UPS, measure for and verify ABSENCE of voltage with a multimeter probe through the holes in the transparent plate for input, bypass, output, neutral, and DC.

    Front View of the UPS

  11. Open the inner door of the UPS.
  12. On the UPS, measure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input/bypass/output/DC busbar before continuing.
    Failure to follow these instructions will result in death or serious injury.
  13. Remove the busbars and insulator parts that connect the UPS to the output transformer cabinet. See Install the Busbars Between the UPS and the Output Transformer Cabinet in a Single Mains System or Install the Busbars Between the UPS and the Output Transformer Cabinet in a Dual Mains System for details. Save all parts for reinstallation.
  14. Remove the busbars and insulator parts that connect the transformer cabinets to each other. See Install the Busbars Between the Transformer Cabinets in a Single Mains System or Install the Busbars Between the Transformer Cabinets in a Dual Mains System for details. Save all parts for reinstallation.
  15. Remove the top brackets and the screws in the front that interconnect the UPS and the transformer cabinets externally. Remove the two special screws that interconnect the UPS and the output transformer cabinet internally. See Position and Interconnect the Transformer Cabinets and the UPS for details. Save all parts for reinstallation.
  16. If external sync is present on the UPS: Remove the transparent protection cover from the external synchronization board 0P4809. The external synchronization board 0P4809 is located on the rear of the front plate. Disconnect the signal cables from the external synchronization board 0P4809.
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Check for absence of voltage for all three signal terminals on the external synchronization board 0P4809. When the external synchronization cables are installed, the terminals on the external synchronization board 0P4809 may be energized. Disconnect the fuse disconnector device at the source before removing the transparent protection cover.
    Failure to follow these instructions will result in death or serious injury.

    Front View of the UPS

  17. Close the inner door of the UPS and reinstall the screws.
  18. Disconnect and remove any signal cables from the UPS.
  19. Remove the seismic front anchoring bracket/front transportation bracket from the UPS and the transformer cabinets. Save for reinstallation.
  20. Close and lock the front door of the UPS.
  21. Raise the feet of the UPS until the casters have full contact with the floor.
  22. Move the UPS out of the way of the transformer cabinets by rolling it on the casters.
    WARNING
    TIPPING hazard
    • The casters of the UPS are exclusively for transport on flat, even, hard, and horizontal surfaces.
    • The casters of the UPS are intended for transport over short distances (i.e. inside the same building).
    • Move at a slow pace and pay close attention on the floor conditions and the balance of the UPS.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  23. Remove the front plates and the transparent plates from the transformer cabinets. See Prepare the Transformer Cabinets for Installation for details.
  24. Measure for and verify ABSENCE of voltage on each input/UPS input/bypass/UPS bypass/output busbar in the transformer cabinets before continuing.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Measure for and verify ABSENCE of voltage on each input/UPS input/bypass/UPS bypass/output busbar before continuing.
    Failure to follow these instructions will result in death or serious injury.

    Single Mains

    Dual Mains

  25. Remove the power cables from the transformer cabinets. See Connect the Power Cables in a Single Mains System or Connect the Power Cables in a Dual Mains System for details.
  26. Perform the following on the transformer cabinets to reposition parts to their original position. See Prepare the Transformer Cabinets for Installation for details.
    1. Remove the left side panel from the leftmost input transformer cabinet and reinstall it on the left side of the UPS.
    2. Reposition the protections cover to their original position on the right side panel of the output transformer cabinet.
    3. Reposition the two rear brackets and the top bracket on each transformer cabinet to their original position.
    4. Reinstall the front plates on the transformer cabinets.
  27. Close and lock the front door of the transformer cabinets.
  28. Raise the feet of the transformer cabinets until the casters have full contact with the floor.
  29. Roll out the output transformer cabinet far enough that you can access the DC cables. Disconnect the DC cables and remove the DC cables. See Position and Interconnect the Transformer Cabinets and the UPS for details.
  30. You can now move the each transformer cabinet by rolling it over the floor on the casters.
    WARNING
    TIPPING hazard
    • The casters of the transformer cabinet are exclusively for transport on flat, even, hard, and horizontal surfaces.
    • The casters of the transformer cabinet are intended for transport over short distances (i.e. inside the same building).
    • Move at a slow pace and pay close attention on the floor conditions and the balance of the transformer cabinet.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  31. If present, remove the rear seismic anchoring bracket from the transformer cabinets and remove the seismic anchors from the floor. Save for reinstallation.
  32. For transport over longer distances or in conditions that are not suitable for the casters of the transformer cabinet:
    WARNING
    Heavy load
    The transformer cabinet is heavy. Take appropriate precautions during handling and preparation for transport/shipment.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
    WARNING
    TIPPING hazard
    For transport over longer distances or in conditions that are not suitable for the casters of the transformer cabinet, ensure:
    • that personnel performing the transport have necessary skill and have received adequate training;
    • to use appropriate tools to safely lift and transport the transformer cabinet;
    • to protect the product against damage by using appropriate protection (like wrapping or packaging).
    Failure to follow these instructions can result in death, serious injury, or equipment damage.

    Transportation requirements:

    • Mount the transformer cabinet in a vertical position in the center of a suitable pallet with minimum pallet dimensions: 1000 mm x 1000 mm (39.4 in x 39.4 in). The pallet must be suitable for the weight of the transformer cabinet. GVIT300 weighs 640 kg (1411 lbs), GVIT500 weighs 795 kg (1753 lbs), GVOT300 weighs 602 kg (1327 lbs), GVOT500 weighs 767 kg (1691 lbs).

    • Use appropriate means of fixation to mount the transformer cabinet to the pallet.

    • The original shipping pallet in combination with the original transportation brackets can be reused, if in undamaged condition.

    DANGER
    TIPPING hazard
    • The transformer cabinet must be appropriately fixed to the pallet immediately after being placed on the pallet.
    • The fixation hardware must be strong enough to withstand vibrations and shocks during loading, transport, and unloading.
    Failure to follow these instructions will result in death or serious injury.
    WARNING
    Unexpected equipment behavior
    Do not lift the transformer cabinet with a forklift/pallet truck directly on the frame as it may bend or damage the frame.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  33. Perform one of the following:
    • Decommission the transformer cabinet, OR
    • Move the transformer cabinet to a new location to install it.
  34. Only for installing the transformer cabinet in a new location: Follow the installation manual to install the transformer cabinet in the new location. See Installation Procedure for Single Mains UPS System or Installation Procedure for Dual Mains UPS System for installation overview. Startup must only be performed by Schneider Electric.
    DANGER
    hAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Startup must only be performed by Schneider Electric.
    Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?