990-91459B-001

Post-Installation Checklist

  1. Verify that the busbars have been installed as instructed.

  2. Verify torque on all electrical connections – see Torque Specifications.

  3. Adjust the settings on the backfeed breaker – see Trip Settings.

  4. Verify the backfeed trip. A Schneider Electric-certified service partner will perform a backfeed breaker test at start-up.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?