990-91379D-001

Start a Battery Test

Prerequisites:

  • The battery breakers are closed.

  • No critical alarms present.

  • The bypass supply must be available.

  • Static bypass operation must be available.

  • The batteries must be more than 50% charged.

  • The runtime available must be more than 4 minutes.

  • The operation mode must be normal operation, eConversion, or ECO mode.

  • The system operation mode must be inverter, eConversion, or ECO mode.

This feature performs a number of tests on the batteries, such as fuse-blown check and weak battery detection. The test will discharge the batteries and use about 10% of the total runtime capacity. Example: If you have 10 minutes of runtime, the test will run for 1 minute. The battery test can be scheduled to run automatically in different time intervals (from weekly and up to once a year).

  1. Select Maintenance > Battery > Start test .
  2. Tap OK on the confirmation screen.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?