990-6196-001

Install the Seismic Anchoring (Option)

  1. Mount the rear anchor(s) to the floor. Use appropriate hardware for the floor type – the hole diameter in the rear anchor is ø14 mm.
  2. Install the rear anchoring bracket on the UPS with the provided M8 bolts.

    Rear View of the UPS

  3. Push the UPS into position so the rear anchoring bracket connects to the rear anchor. The front anchoring bracket is installed in the final installation steps.

    Rear View of the UPS

QR code for this page

Was this helpful?