990-5913E-001

Decommission or Move the Classic Battery Cabinet to a New Location

  1. Open the door(s). On GVSCBC10A2 and GVSCBC10B2, remove two screws to open the left door.
  2. Lockout/Tagout the battery breaker in the OFF (open) position.
  3. Remove the breaker protection plates.

    GVSCBC7C, GVSCBC7D, GVSCBC7E

    GVSCBC10A2, GVSCBC10B2

  4. Remove the terminal cover from the left side of the battery breaker.
  5. Disconnect and remove the DC cables and PE cable from the battery breaker.

    GVSCBC7C, GVSCBC7D, GVSCBC7E

    GVSCBC10A2, GVSCBC10B2

  6. Disconnect and remove the interconnection copper bars or interconnection cables between the batteries on each shelf. Disconnect and remove the battery cables from the right side of the battery breaker. Refer to the connection diagram on the inside of the front door of the classic battery cabinet.
    DANGER
    Hazard of electric shock, explosion, or arc flash
    Batteries can present a risk of electric shock and high short-circuit current. The following precautions must be observed when working on batteries:
    • Remove watches, rings, or other metal objects.
    • Use tools with insulated handles.
    • Wear protective glasses, gloves, and boots.
    • Do not lay tools or metal parts on top of batteries.
    • Disconnect the charging source prior to connecting or disconnecting battery terminals.
    • Determine if the battery is inadvertently grounded. If inadvertently grounded, remove source from ground. Contact with any part of a grounded battery can result in electric shock and burns by high short-circuit current. The likelihood of such shock can be reduced if such grounds are removed during installation and maintenance by a skilled person (applicable to equipment and remote battery supplies not having a grounded supply circuit).
    Failure to follow these instructions will result in death or serious injury.
  7. Remove the batteries from the shelves. Recycle or reuse the batteries as appropriate.
    DANGER
    HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
    Servicing of batteries must only be performed or supervised by qualified personnel knowledgeable of batteries and the required precautions. Keep unqualified personnel away from batteries.
    • Recycle lead-acid batteries correctly. Batteries contain lead and dilute sulfuric acid.
    • Dispose of the batteries in accordance with country and local regulations.
    Failure to follow these instructions will result in death or serious injury.
  8. Reinstall the terminal cover on the left side of the battery breaker.
  9. Disconnect and remove any signal cables from the classic battery cabinet.
  10. Reinstall the breaker protection plates.

    GVSCBC7C, GVSCBC7D, GVSCBC7E

    GVSCBC10A2, GVSCBC10B2

  11. Close the door(s). On GVSCBC10A2 and GVSCBC10B2, install two screws to close the left door.

    GVSCBC10A2, GVSCBC10B2

  12. Remove the kick plates from the front, rear, and sides of the classic battery cabinet.
  13. Lift the classic battery cabinet from the left or right side with a pallet truck.
    WARNING
    TIPPING hazard
    • Do not lift the cabinet with a forklift. Use a pallet truck
    • Do not lift the cabinet from the front or from the rear. Lift from the left or right side.
    Failure to follow these instructions can result in death, serious injury, or equipment damage.
  14. Perform one of the following:
    • Decommission the classic battery cabinet, OR
    • Move the classic battery cabinet to a new location to install it.
  15. Only for installing the classic battery cabinet in new a location: Reinstall the batteries in the classic battery cabinet after moving it to the new location. Follow the installation manual to install battery interconnections, signal cables, power cables, etc. See Installation Procedure for installation overview.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?