990-91317F-001

Derating Due to Load Power Factor

0.7 leading to 0.7 lagging without derating.

UPS rating UPS output
Lagging Leading
PF=1 PF=0.7 PF=0.8 PF=0.9 PF=0.9 PF=0.8 PF=0.7
10 kVA/kW

10 kVA / 7 kW

10 kVA / 8 kW

10 kVA / 9 kW

10 kVA / 9 kW

10 kVA / 8 kW

10 kVA / 7 kW

15 kVA/kW

15 kVA / 10.5 kW

15 kVA / 12 kW

15 kVA / 13.5 kW

15 kVA / 13.5 kW

15 kVA / 12 kW

15 kVA / 10.5 kW

20 kVA/kW

20 kVA / 14 kW

20 kVA / 16 kW

20 kVA / 18 kW

20 kVA / 18 kW

20 kVA / 16 kW

20 kVA / 14 kW

30 kVA/kW

30 kVA / 21 kW

30 kVA / 24 kW

30 kVA / 27 kW

30 kVA / 27 kW

30 kVA / 24 kW

30 kVA / 21 kW

40 kVA/kW

40 kVA / 28 kW

40 kVA / 32 kW

40 kVA / 36 kW

40 kVA / 36 kW

40 kVA / 32 kW

40 kVA / 28 kW

50 kVA/kW

50 kVA / 35 kW

50 kVA / 40 kW

50 kVA / 45 kW

50 kVA / 45 kW

50 kVA / 40 kW

50 kVA / 35 kW

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?