990-5910F-001

Enable SNMP Protocols

  1. Access the network management interface by its IP address (or its DNS name, if a DNS name is configured).
  2. Enter the user name and password. The default user name and password is apc. You will be prompted to change this password on the first login.
  3. To enable SNMPv1 protocol:
    1. Go to Configuration > Network > SNMPv1 > Access , select Enable and click on Apply.
    2. Go to Configuration > Network > SNMPv1 > Access Control and set up the parameters.
  4. To enable SNMPv3 protocol:
    1. Go to Configuration > Network > SNMPv3 > Access , select Enable and click on Apply.
    2. Go to Configuration > Network > SNMPv3 > Access Control and set up the parameters.
    3. Go to Configuration > Network > SNMPv3 > User Profiles and set up the parameters.
NOTE: The SNMPv1 or SNMPv3 settings must match your settings on the EcoStruxure IT Gateway or StruxureWare Data Center Expert for the network management card 4 to communicate correctly with EcoStruxure IT Gateway or StruxureWare Data Center Expert.
QR code for this page

Was this helpful?