990-5910F-001

Status LEDs on the Modular Battery Cabinet

Remove the front door/front panel from the modular battery cabinet to see the status LEDs for the battery strings.
  • Green LED means that this battery string is OK.

  • Off LED means that the modular battery cabinet is powered off or that no battery modules are installed for this battery string.

  • Red LED means that this battery string is incomplete (not all four required battery modules are connected).

  • Flashing red LED means that an alarm is present for this battery string.

See View the Modular Battery Status and View the Logs for more alarm information. See Replace or Install a Modular Battery String on how to replace a battery string.
QR code for this page

Was this helpful?