990-91263A-001

Interconnect Modular Battery Cabinet 1 and the Adjacent UPS for External Batteries

  1. Push the UPS into place.
  2. Install the three interconnection clamps on modular battery cabinet 1.

    Rear View of Modular Battery Cabinet 1

  3. Fasten the signal cables (0W13069 and 0W13070) from optional kit GVSOPT030 on the right side of modular battery cabinet 1 with the provided cable ties. Place the cable ends temporarily in the top and in the bottom shelf of modular battery cabinet 1, so the cables do not get damaged during the interconnection with the UPS. Cable connections are described in Connect the Signal Cables.
  4. Fasten the DC cables and the PE cable from optional kit GVSOPT030 on the right side of modular battery cabinet 1 with the provided cable ties. Place the cable ends temporarily in the top and in the bottom shelf of modular battery cabinet 1, so the cables do not get damaged during the interconnection with the UPS. Cable connections are described in Connect the Power Cables for a UPS Rated for Maximum 50 kW or Connect the Power Cables for a UPS Rated over 50 kW.

    Adjacent UPS for External Batteries Rated for Maximum 50 kW

    Adjacent UPS for External Batteries Rated over 50 kW

  5. Align modular battery cabinet 1 with the UPS. Push in modular battery cabinet 1 until the holes for the front interconnection screws are aligned with the holes in the UPS. The interconnection clamps will connect to the UPS when in the correct position.
  6. Install the three interconnection screws between modular battery cabinet 1 and the UPS.

    Modular Battery Cabinet 1 and the UPS for External Batteries

  7. Push the baying cover down between modular battery cabinet 1 and the UPS.
QR code for this page

Was this helpful?