990-6161A-001

Interconnect the Modular Battery Cabinets

Use installation kit 0H-220042 and optional seismic kit GVSOPT016 for this procedure.
  1. Push the rightmost modular battery cabinet into place.
    1. Lower the front and rear leveling feet on the modular battery cabinet with a wrench until they connect with the floor. Use a bubble-leveler to check that the cabinet is level.
    NOTICE
    Risk of Equipment damage
    Do not move the cabinet after the leveling feet have been lowered.
    Failure to follow these instructions can result in equipment damage.
  2. Repeat the previous step for each modular battery cabinet.
  3. Only for seismic anchoring: Install the two interconnection brackets between the modular battery cabinets.
  4. Install the interconnection screws between the modular battery cabinets.
  5. Install the baying covers in the top and bottom between the modular battery cabinet.
QR code for this page

Was this helpful?