990-91141K-001

Leakage Current

380/400/415 V UPS system 4-wire installation at 100% load

UPS rating Leakage current
20-50 kW 62 mA
60-100 kW 67 mA
120-150 kW 91 mA
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?