Prepare the Maintenance Bypass Panel for Cables
![]() |
---|
hazard of electric shock, explosion, or arc flash
Do not drill or punch holes with the gland plates installed and do not drill or punch
holes in close proximity to the maintenance bypass cabinet.
Failure to follow these instructions will result in death or serious injury.
|
- Loosen the six bolts from the bottom gland plate and remove the gland plate.
- Drill or punch holes for cables or grommets.
DANGER
hazard of electric shock, explosion, or arc flashEnsure that there are no sharp edges that can damage the cables.Failure to follow these instructions will result in death or serious injury. - Install grommets (if applicable) and reinstall the gland plate(s).