990–5947A–016

Spesifikasi Torsi

Ukuran baut Torsi
M4 1,7 Nm (1,25 lb-ft)
M6 5 Nm (3,69 lb-ft)
M8 17,5 Nm (12,91 lb-ft)
M10 30 Nm (22 lb-ft)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Apakah ini membantu?