990-5910F-001

View the Modular Battery Status

  1. Select Status > Battery > Details. An overview of the modular battery solution is shown. You can see the battery breaker status for each modular battery cabinet and for the modular batteries inside the UPS (only available for UPS models for internal batteries). If the battery symbol is red, it means that an alarm exists for modular batteries in the modular battery cabinet or in the UPS. The temperature shown on this screen is the highest battery string temperature measured in the modular battery cabinet/UPS.
  2. Tap the battery symbol named Internal (in UPS) (only present for UPS models for internal batteries) to see the information for modular batteries in the UPS or tap the battery symbol named ModBC # x to see the information for modular battery cabinet x. You will then be able to see details for each battery string such as number of installed battery modules, alarm presence, temperature for each battery string, and battery module type.
QR code for this page

Was this helpful?