990-91111L-037

漏电电流

380/400/415 V UPS 系统 4 线安装,100% 负载

UPS 额定值 漏电电流
20-50 kW 62 mA
60-100 kW 67 mA
120-150 kW 91 mA
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?