990-91264A-001

Final Installation

  1. Close the inner door and fasten it with the screws.
  2. Add labels to the breaker indicator lamps, the breakers, and the diagram label according to your system. The labels are provided with this manual.

    Labels in Single Mains System

    Labels in Dual Mains System

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?