7EN02-0438-14

Meter overview

 

A

Digital input

 

B

Digital output

 

C

Communication port

 

D

Communication LED

 

E

Display with white backlight for measurement and configuration

 

F

Scroll through screens or a list of options

 

G

Confirm entry or access more screens

 

H

Cancel and go back to previous screen

 

I

V1, V2, V3, Vn, I1, I2, I3

 

J

Energy pulse LED

NOTE:
  • Within 24000/x, x is the primary current for iEM3455 / iEM3465.

  • The meter constant for iEM3555 / iEM3565 is 5.

  • For iEM3455C1, x is 2 Wh/pulse.

  • For iEM3455C2, x is 5 Wh/pulse.

 

K

Status LED: on / off / error

 

L

Sealing points (3)

 

M

Sealable covers (2)

 

NOTE: The sealable covers must be installed and sealed to the sealing points with the steel cable. Use steel cable with 1.6 mm (1/16 in) diameter and 152.4 mm (6 in) adjustable length for sealing.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?