7EN02-0438-14

Power system wiring

iEM3455 / iEM3465 / iEM3555 / iEM3565

1PH

1PH2W L-N ≤ 240 V L-N

1PH2W L-L ≤ 415 V L-L

1PH3W L-L-N ≤ 240 V L-N
≤ 480 V L-L

1PH3W multi L-N 2LVCS ≤ 240 V L-N

1PH4W multi L-N 3LVCS ≤ 240 V L-N

3PH3W

1LVCS ≤ 480 V L-L

2LVCS ≤ 480 V L-L

3LVCS ≤ 480 V L-L

3PH3W

2VT, 1LVCS

2VT, 2LVCS

2VT, 3LVCS

3PH4W

1LVCS ≤ 277 V L-N
≤ 480 V L-L

2LVCS ≤ 277 V L-N
≤ 480 V L-L

3LVCS ≤ 277 V L-N
≤ 480 V L-L

3PH4W

3VT, 1LVCS

3VT, 2LVCS

3VT, 3LVCS

250 mA fuses and disconnect switch

LVCS with insulation rated for the installation voltage and the installation/ measurement category

NOTE: LVCS refers to both LVCT and Rogowski coil.

VT primary fuses and disconnect switch

  • indicates wiring for a balanced system
  • + indicates white wire
  • - indicates black wire

Clearly label the device’s disconnect circuit mechanism and install it within easy reach of the operator.

Fuses / circuit breakers must be rated for the installation voltage and sized for the available fault current. Fuse for neutral is required if the source neutral is not grounded.

iEM3455C1 / iEM3455C2

3PH4W

3LVCT

250 mA fuses and disconnect switch

LVCT with insulation rated for the installation voltage and the installation/ measurement category

VT primary fuses and disconnect switch

  • + indicates white wire
  • - indicates black wire

Clearly label the device’s disconnect circuit mechanism and install it within easy reach of the operator.

Fuses / circuit breakers must be rated for the installation voltage and sized for the available fault current. Fuse for neutral is required if the source neutral is not grounded.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?