DOCA0147EN-04

EIFE Embedded Ethernet Interface for One MasterPact MTZ Drawout Circuit Breaker

The EIFE Embedded Ethernet interface for one MasterPact MTZ drawout circuit breaker (or EIFE interface) enables one MasterPact MTZ drawout circuit breaker to be connected to an Ethernet network.

It provides:

  • Digital access to all the data that is delivered by the MicroLogic X control unit of the MasterPact MTZ circuit breaker.

  • Information about the intelligent modular unit (IMU) system

It also monitors the three positions of the circuit breaker in the cradle:

  • Cradle connected

  • Cradle disconnected

  • Cradle test position

QR code for this page

Was this helpful?