DOCA0147EN-04

Firmware Update Policy

Firmware update is recommended to benefit from the latest features and potential bug fixes. Do not update the firmware to the latest version, if the latest features are not required for your application and no bug fixes are provided.

Use this release note to confirm if an update to the latest version of the IFE/EIFE firmware is relevant for your application.

For more information on the firmware update policy and the firmware compatibility between devices, refer to DOCA0155EN MicroLogic Trip and Control Units - Firmware History.

QR code for this page

Was this helpful?