DOCA0147EN-04

Firmware Version 003.005.003

New Features

New features in this firmware version for IFE server and IFE/EIFE interface:

  • Added the MasterPact MTZ circuit breakers as discoverable devices.

  • Added the integration of secure email.

Bugs Fixed

Bugs fixed in this firmware version for IFE server and IFE/EIFE interface:

  • IFE time and date were not well synchronized with the SNTP server.

  • Refresh of data on IFE device stopped after a few hours of use.

  • IP filtering was disabled after a firmware update of IFE devices.

  • IFE device and IO module ULP communication did not share the correct cradle status when powered up with a device in disconnected position.

QR code for this page

Was this helpful?