DOCA0147EN-04

Firmware Version 003.006.011

New Features

New features in this firmware version for IFE server and IFE/EIFE interface:

  • Added access through Modbus registers to the trip cause data for MasterPact MTZ circuit breakers

  • Added support of alpha-numeric passwords for IFE webpages

New features in this firmware version for IFE server and IFE interface:

  • Added support for the internal battery that maintains the date and time settings of the real-time clock (RTC) during a power loss (references LV434001 and LV434002)

  • Added compatibility with ULP cables up to 20 m (65 ft) in length

  • Added alarm support for the MicroLogic P and H advanced protection settings, allowing an alarm email to be sent

  • Added discovery from IFE webpages of devices equipped with non-communicating trip units, through BCM or BSCM module (e.g. NSX non-communicating MicroLogic with BSCM module), for device status display only

  • Added compatibility with new MicroLogic 7 trip units for ComPact NSX circuit breakers

New features in this firmware version for IFE server:

  • Added Integration of Acti9 Smartlink SI D as a remote device

  • Updated Modbus end-of-line termination default value in webpage for easier default configuration

NOTE: The Schneider Electric automatic email profile is not available now. You have to use your own SMTP server.

Bugs Fixed

Bugs fixed in this firmware version for IFE server and IFE/EIFE interface:

  • FTP server could not be enabled in Italian language

Bugs fixed in this firmware version for IFE server and IFE interface:

  • BCM firmware update was not performed when IFE device closed connection in DHCP mode.

QR code for this page

Was this helpful?