DOCA0147EN-04

Firmware Version 003.009.010

New Features

New features in this firmware version for IFE/EIFE interface:

  • Added the following maintenance features, available with a MicroLogic X control unit with firmware version 003.011.000 or higher:

    • New events for contact wear ratio

    • New events for type of preventive maintenance to be performed

  • Added access through Modbus registers to the following data for MasterPact MTZ circuit breakers:

    • Average peak current demand

    • Minimum and maximum values of real-time measurements

    • Energy per phase values

    • Main settings of the active setting group of current protection functions

NOTE: The configuration of the connection to EcoStruxure Facility Expert is not available now. You can use Enerlin'X COM'X energy servers to configure the connection to EcoStruxure Facility Expert.

Bugs Fixed

Bugs fixed in this firmware version for IFE/EIFE interface:

  • IFE/EIFE interface lost its clock master status when SNTP server did not answer.

  • IFE/EIFE interface restarted when discovery packet from Satchwell Sigma BMS platform was received.

QR code for this page

Was this helpful?