DOCA0147EN-04

IFE Ethernet Interface for One Circuit Breaker

When an intelligent modular unit (IMU) contains a circuit breaker equipped with a communicating MicroLogic trip unit, the IFE Ethernet interface for one circuit breaker (IFE interface) enables the IMU to be connected to an Ethernet network. Each circuit breaker has its own IFE interface and a corresponding IP address.

The IFE interface is compatible with the following ranges of circuit breakers:

  • MasterPact MTZ circuit breakers

  • MasterPact NT/NW circuit breakers

  • ComPact NS circuit breakers

  • ComPact NSX circuit breakers

  • PowerPact P- and R-frame circuit breakers

  • PowerPact H-, J-, and L-frame circuit breakers

The IFE interface with part number LV434001 or LV434010 is an Ethernet interface for the circuit breaker in the IMU.

QR code for this page

Was this helpful?