DOCA0147EN-04

IFE Switchboard Server

When an intelligent modular unit (IMU) contains a circuit breaker equipped with a communicating MicroLogic trip unit, the IFE Ethernet switchboard server (IFE server) enables the IMU to be connected to an Ethernet network. Each circuit breaker has its own IFE server and a corresponding IP address.

The IFE server is compatible with the following ranges of circuit breakers:

  • MasterPact MTZ circuit breakers

  • MasterPact NT/NW circuit breakers

  • ComPact NS circuit breakers

  • ComPact NSX circuit breakers

  • PowerPact P- and R-frame circuit breakers

  • PowerPact H-, J-, and L-frame circuit breakers

The IFE server with part number LV434002 or LV434011 is an Ethernet interface for the circuit breaker in the IMU and a server for Modbus-SL (serial line) connected devices.

QR code for this page

Was this helpful?