DOCA0147EN-07

Firmware Version 003.006.011

New Features

New features in this firmware version for IFE/EIFE interface:

  • Added access through Modbus registers to the trip cause data for MasterPact MTZ circuit breakers

  • Added support of alpha-numeric passwords for IFE webpages

New features in this firmware version for IFE interface:

  • Added support for the internal battery that maintains the date and time settings of the real-time clock (RTC) during a power loss (reference LV434001)

  • Added compatibility with ULP cables up to 20 m (65 ft) in length

  • Added alarm support for the MicroLogic P and H advanced protection settings, allowing an alarm email to be sent

  • Added discovery from IFE webpages of devices equipped with non-communicating trip units, through BCM or BSCM module (e.g. NSX non-communicating MicroLogic with BSCM module), for device status display only

  • Added compatibility with new MicroLogic 7 trip units for ComPacT NSX circuit breakers

Bugs Fixed

Bugs fixed in this firmware version for IFE/EIFE interface:

  • FTP server could not be enabled in Italian language

Bugs fixed in this firmware version for IFE interface:

  • BCM firmware update was not performed when IFE device closed connection in DHCP mode.

QR code for this page

Was this helpful?