Schematics with MasterPacT NT/NW , ComPacT NS, PowerPacT P- and R-Frame Circuit Breakers
Description
Depending on the type of circuit breaker used, connect the IFE interface to the circuit breaker using one of the following configurations:
-
Connection of the IFE interface to a fixed manually-operated circuit breaker with a BCM ULP module:
-
ComPacT NS 630b-3200 circuit beakers
-
PowerPacT P- or R-Frame circuit
-
-
Connection of the IFE interface to a fixed electrically-operated circuit breaker with a BCM ULP module:
-
MasterPacT NT/NW circuit beakers
-
ComPacT NS 630b-1600 circuit beakers
-
PowerPacT P-Frame circuit breakers
-
-
Connection of the IFE interface to a drawout circuit breaker with a BCM ULP module and its respective IO module:
-
MasterPacT NT/NW circuit beakers
-
ComPacT NS 630b-1600 circuit beakers
-
PowerPacT P-Frame circuit breakers
-
For more information, refer to the ULP System User Guide in Related Documents.
ULP Connection
NOTICE |
---|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All connection configurations require the BCM ULP cord.
Connection of the IFE Interface to a Fixed Manually-Operated Circuit Breakers
Applicable for:
-
ComPacT NS 630b-3200 circuit beakers
-
PowerPacT P- or R-Frame circuit
A |
IFE Ethernet interface for one circuit breaker |
B |
ULP line termination |
C |
Circuit breaker BCM ULP cord |
D |
BCM ULP circuit breaker communication module |
E |
Fixed manually-operated circuit breaker |
Connection of the IFE Interface to a Fixed Electrically-Operated Circuit Breakers
Applicable for:
-
MasterPacT NT/NW circuit beakers
-
ComPacT NS 630b-1600 circuit beakers
-
PowerPacT P-Frame circuit breakers

A |
IFE Ethernet interface for one circuit breaker |
B |
ULP line termination |
C |
Circuit breaker BCM ULP cord |
D |
Fixed terminal block |
E |
BCM ULP circuit breaker communication module |
F |
Fixed electrically-operated circuit breaker |
Connection of the IFE Interface to the Drawout Circuit Breakers
Applicable for:
-
MasterPacT NT/NW circuit beakers
-
ComPacT NS 630b-1600 circuit beakers
-
PowerPacT P-Frame circuit breakers

A |
IFE Ethernet interface for one circuit breaker |
B |
ULP line termination |
C |
RJ45 plug/plug ULP cord |
D |
Circuit breaker BCM ULP cord |
E |
Circuit breaker disconnected position contact (CD) |
F |
Circuit breaker cradle |
G |
BCM ULP circuit breaker communication module |
H |
Drawout circuit breaker |
I |
Drawout terminal block |
J |
Circuit breaker connected position contact (CE) |
K |
Circuit breaker test position contact (CT) |
L |
IO input/output application module for one circuit breaker |