DOCA0142EN-07

Firmware Update

Description

Use the latest version of EcoStruxure Power Commission software for all firmware updates.

The latest version of IFE firmware and IFE webpages are updated in a single operation through EcoStruxure Power Commission software.

For more information on IFE firmware versions, refer to Enerlin'X IFE Interface Firmware Release Note.

NOTICE
LOSS OF DATA
  • Ensure that you take backup of the data log files before updating the firmware. The data log entries of the IFE interface may be lost when the IFE firmware is updated.
  • Ensure that you take backup of data present in User Accounts and Email Events sections of IFE webpages.
  • Ensure that after firmware upgrade, you restore the User Accounts and Email Events configuration on IFE webpages.
Failure to follow these instructions can result in permanent loss of data.

After updating the firmware of one device in the IMU, use the latest version of EcoStruxure Power Commission software to check the firmware compatibility between the IMU devices. The Firmware Update table helps you to diagnose and identify all discrepancy issues between the IMU devices. This table also provides the recommended actions relevant to the detected discrepancies.

Checking the Firmware Version

You can find the firmware version of the devices in the IMU by using:

  • EcoStruxure Power Commission software, refer to the EcoStruxure Power Commission Online Help

    DOCA0069EN
    .

  • IFE webpages, see the procedure below.

Step

Action

Result

1

Open the web browser and log in to the IFE webpage.

Opens the IFE home page.

2

  • For checking the firmware version 004 and later: go to the DIAGNOSTICS menu, and in the IFE page, locate the firmware version.

  • For checking the firmware version up to 003: go to the Diagnostics menu, and in the Device Information page, locate the firmware version.

NOTE: If you have updated the firmware recently, press F5 to refresh the webpage and update the displayed firmware number. The new authentication may be required to access the webpages.

Determines the firmware version of the IFE interface.

Updating the Firmware and Webpages, Using EcoStruxure Power Commission Software

For more information, refer to the EcoStruxure Power Commission Online Help

DOCA0069EN
.

The EcoStruxure Power Commission software is available at www.se.com.

QR code for this page

Was this helpful?