Device List
Description
The circuit breaker connected to the IFE interface is automatically detected. Click the Apply button to add it in the device list.
Device List Parameters
Parameters |
Description |
Settings |
---|---|---|
|
Displays the device IP address. |
– |
|
Indicates if the IP device is a gateway or not. NOTE: Gateway check box is always cleared
for IFE interface.
|
– |
|
Displays the Modbus address of the IFE interface. NOTE: The
text box is unavailable to edit. |
255 (fixed) |
|
Allows you to enter the name for IFE interface. NOTE:
|
The IFE device name can have up to 64 ASCII characters with the following characters: A–Z, a–z, 0–9, and -. However, - cannot be used at the end of the name. NOTE:
|
|
Displays the connection type (ULP). NOTE: The
field is unavailable
to edit. |
port |
|
Automatically displays the device type discovered on the ULP system. NOTE: The
field is auto-detected and it is unavailable to edit. |
– |
|
Allows you to enter the name for the discovered devices. |
The device name can have up to:
The allowed characters are: A–Z, a–z, 0–9, and -. However, - cannot be used at the end of the name. |
|
Displays the local address of the device connected to the IFE interface. |
255 (Fixed) |
|
Allows you to save device list configuration. |
– |
|
This operation is not available. |
– |
|
Allows you to edit the device name. |
– |