Communication Check
Automated Communication Check
While browsing the real-time data views, the IFE server has an automated communication check that runs every 15 minutes by default. To change the timing, refer to Preferences. This check verifies the communication health of all the devices configured on the IFE server, and attempts to re-establish the communication to any device marked out of service within the current browser session.
Manual Communication Check
In certain cases, there is no need to wait for the automated communications check interval and need to force the check to run manually.
|
Step |
Action |
Result |
|---|---|---|
|
1 |
From the IFE menu bar, click . |
Opens the menu. |
|
2 |
From the menu, in the submenu, click . |
Opens the page. |
|
3 |
Click . |
Runs a communications check. The communicating device displays:
A device that is not communicating display:
|