DOCA0084EN-12

General

Device Physical Location

Step

Action

Result

1

From the IFE menu bar, click Configuration & Settings.

Opens the Configuration & Settings menu.

2

From the Configuration & Settings menu, in the General submenu, click Device Physical Location.

Opens the Device Physical Location page.

3

In Device Physical Location webpage, click Blink ON.

Sets the IFE server in test mode and the LED blinks in ULP pattern with 1 second ON and 1 second OFF.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?