Redundancy-RSTP Ports
Description
The REDUNDANCY-RSTP PORTS page displays the diagnostic data of RSTP ports.
The users with installer or engineer roles can make changes to the Diagnostics page settings.
Navigation to the REDUNDANCY-RSTP PORTS Page
To view the REDUNDANCY-RSTP PORTS page, click .
Port 1 and Port 2 Parameters
|
Parameter |
Description |
|---|---|
|
State |
Current state of the port. By default, it is disabled, blocking, and forwarding. NOTE: Other
states like listening, learning are intermediate states which are
not visible to the user.
|
|
Role |
Current role of the port in the ring. If the port state is disabled, the role can be either Root or Designated. If the port state is disabled (Ethernet link is down) then the Role is Unknown. |
|
Priority |
The value of the port priority is contained in Port Identifier. All ports of a bridge will have a port identifier with format: [1 byte port number][1 byte port priority]. NOTE: Following points are provided for understanding
the usage of port priority (port identifier).
|
|
Port Path Cost |
The contribution of this port to the path cost of paths towards the Root bridge which includes this port. |
|
Received RST (BPDUs) |
Total number of RSTP BPDUs received by this port since the last reset counters. |
|
Transmitted RST (BPDUs) |
Total number of RSTP BPDUs transmitted by this port since the last reset counters. |
|
Received TCN (BPDUs) |
Total number of Topology Change BPDUs received by this port since the last reset counters. |
|
Transmitted TCN (BPDUs) |
Total number of Topology Change BPDUs transmitted by this port since the last reset counters. |
|
Click Reset Counters to reset to 0 the statistics values. If the IFE server is switched off or if it is reset due to a configuration change or another event, the statistics values are reset to 0. |
|