DOCA0148EN-04

Firmware Version 003.010.005

New Features

  • Added access through Modbus registers to the following data for MasterPact MTZ circuit breakers:
    • IDMTL protection trip

    • Over/Under frequency trip

    • Directional overcurrent trip

    • Discrepancy between display and MicroLogic

Bugs Fixed

  • Modbus TCP communication was lost due to serial driver issue.

  • When IP Filtering was enabled as Read only, the Modbus function Scattered read was blocked.

QR code for this page

Was this helpful?