7EN02-0422-01

Inducing one dummy fault

  1. Induce a dummy fault on one of the channel. For example: Channel 12.

    The device displays the insulation alarm on the detected channel 12, the alarm LED turns ON, and the no alarm LED turns OFF.

    Channel 12 displaying fault in Commissioning screen is as follows:

  2. Recover the dummy fault on channel 12.

    The device returns to toroid detected state, the alarm LED turns OFF, and the no alarm LED turns ON.

    The Commissioning screen in toroid detected and no fault state is as follows:

QR code for this page

Was this helpful?