7EN02-0421-03

Application (App)

The device is designed and tested to be compliant with different applications, which can be monitored. The device is compliant with the following applications:

  • Power circuits: industrial or marine applications that contain power loads and power electronics such as speed drives, inverters, or rectifiers.

  • Control circuits: auxiliary control circuits used to drive power systems. These circuits contain sensitive loads such as PLCs, IOs, or sensors.

To optimize the measurement performance of the device according to the application, you can set the application parameter depending on the type of application on which the device is installed:

Parameter Value Application
Power C. (Default) Power circuits
Control C. Control circuits

NOTE: Ensure that the selected parameter value is same as IMD network parameter value. For example, if you select Power C. in the device make sure that in IMD, the App value is also set to Power C.. If the values are not same, the device might not work as expected.
QR code for this page

Was this helpful?