7EN02-0421-03

Commissioning

The device must be commissioned so that the device can detect toroids and identify the insulation fault in the respective toroids.

Performing commissioning is mandatory when you:

  • Install a new device

  • Install one or more toroid to an installed device

  • Remove one of more toroid from an installed device

  • Replace the toroid with a different type. (Example: Replace TA30 type by PA50 type)

  • Replace the device

Performing commissioning is not required when you reconnect or replace a toroid with the same type of toroid.

The device offers the following commissioning modes:

  • Automatic

  • Manual

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?