7EN02-0421-03

Insulation alarm (Ins. Alarm) thresholds

You can set the threshold value as per the level of insulation of the application you monitor.

The allowed values for this parameter are from 0.2 kΩ to 200 kΩ. The default value is 10 kΩ. This value can be set for 12 channels individually or together.

When the device is powered up, it retrieves the last insulation alarm threshold values recorded.

An insulation alarm is cleared when the insulation level reaches 20% above the threshold.

QR code for this page

Was this helpful?