DOCA0146EN-07

Firmware Version 003.000.012

New Features

@Updated D1
A new IFM interface with part number LV434000 is introduced:

  • With backward compatibility with existing IFM interfaces with part numbers TRV00210 and STRV00210.

  • With the following new features:

    • Compatible with MasterPacT MTZ circuit breakers.

    • Supports discovery and firmware update with EcoStruxure Power Commission software.

    • Improved logic in updating frequency metering values based on quality.

    • Improved logic in managing broadcast commands sent through command interface.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?